InfiniiMax Oscilloscope Probes Impact on (ROHS) Lead–Free Compliance

Notas de Aplicação

Some Keysight Technologies, Inc. InfiniiMax oscilloscope probe heads are intended for soldering to the device under test. These include the following:

– E2677A differential solder-in probe head

– E2679A single-ended solder-in probe head

– N5381A 12-GHz differential solder-in probe head

– N5425A ZIF probe head (with either the N5426A ZIF tip or the N5451A long-wire ZIF tip)

In addition, the Keysight E2678A differential socketed probe head is supplied with resistors that may be soldered to the device under test.