Solar Cell Efficiency

Notas de Aplicação

This application note demonstrates how DiffractMOD and Multi-Variable Optimization and Scanning Tool (MOST) can be used to determine if the addition of diffractive reflection grating and Distributed Bragg Reflector (DBR) to the design as described in a previous study effectively traps light within the structure resulting in a significant efficiency improvement. The structure consists of a single-layer anti-reflection (AR) coating, a silicon absorber with frequency-dependent absorption, a rectangular diffraction grating and a Si/SiO2 DBR reflector.

 

DiffractMOD, based on Rigorous Coupled Wave Analysis (RCWA), is used to calculate the absorption spectrum by modeling the full electromagnetic response of the device. MOST then processes the spectrum to compute solar cell efficiency and performs parameter scans to optimize the structure.

 

Initial results show base efficiencies of ~12% and ~15% for 5 μm and 10 μm silicon thicknesses without the grating or DBR. When the grating and DBR are included, the optimized structures reach efficiencies of ~17% and ~19%, demonstrating that the light-trapping design can significantly enhance device performance.