Notas de Aplicação
This application note demonstrates how the RSoft Solar Cell Utility, in combination with MOST, DiffractMOD, and LaserMOD, can be used to evaluate the performance of a multi-junction organic solar cell.
Key inputs include global collection efficiency (GCE), open circuit voltage (VOC), and filling factor (FF). In this example, the GCE is determined using the ideal diode model and experimental data from a published study, while other parameters are also taken from reference values.
Simulation results show good agreement with published data, demonstrating the ability of the RSoft tool suite to accurately model the optical and electrical performance of multi-junction organic solar cells.
O que você está procurando?