キーサイト公式
再生品ストア

Keysight Oscilloscope Glossary

What is a Function Generator?

Table of contents
「最終更新日」: 12月 11, 2025
Callum Reed
Used Equipment Store Marketing Manager
ご意見・ご感想をお寄せください
Stay Up to Date on Used Equipment!

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Get Email Updates
Second-Hand. First-Class.

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Why Buy From Keysight

Introduction

This device performs a critical role in electronic engineering and is a cornerstone for testing, designing, and analyzing electronic devices. Let's dive into the fascinating world of function generators, their features, applications, and why they're a must-have for anyone involved in electronics.

Function generators and signal or waveform generators are electronic devices that produce various types of repetitive waveforms over a broad range of frequencies. These waveforms can include sine waves, square waves, triangular waves, and sawtooth patterns. Function generators are essentially the heartbeat of many electronic circuit designs and testing procedures. They provide the "input" that helps engineers study and analyze the "output" of their designs.

Buy Signal, Function + Waveform Generators at a Great Discount

すべてを見る Signal Generators
  • Like-new Condition
  • Updated Firmware
  • Full Calibration
  • New Accessories
  • Like-new Warranty
  • Customization possible

Learn more

  • Savings of up to 90%
  • Working Condition
  • Calibrated or Tested
  • 30-Day Right-of-Return
  • No Customization
  • Shipping to limited countries

Learn more

Select up to 3 instruments to compare

Cancel
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at

The Anatomy of a Function Generator

Although function generators can differ in design and complexity, the primary components are quite consistent. Here's a brief outline of what makes up a function generator:

  • Frequency Control: This component adjusts the rate at which the waveform repeats.
  • Amplitude Control: This alters the signal's strength or magnitude.
  • Waveform Selector: Allows the user to select the type of waveform to be generated.
  • DC Offset Control: This changes the average amplitude of the waveform.
  • Output Connector: This is where the generated signal exits the device to be used in an external circuit.

Key Takeaway

Function generators are vital tools in electronic engineering, delivering diverse waveforms crucial for testing and design. Their broad range of applications, from specialized engineering fields to everyday devices, underscores their importance in our technologically driven world.

Function Generator Applications

The application of function generators is quite broad and diversified, largely driven by the variety of waveforms they can produce and the range of frequencies at which these waveforms can be generated. Here are a few applications that showcase the versatility of function generators:

  1. Testing Electronic Equipment: Function generators are used to simulate various conditions under which an electronic device may operate. This aids in performance testing and troubleshooting.
  2. Signal Processing Research: These generators are also invaluable in signal processing research, where different waveforms at different frequencies are often required.
  3. Communications: In communications, function generators are used for testing, troubleshooting, and repairing communication equipment.
  4. Education: In educational settings, function generators are practical tools for teaching the fundamentals of waveforms and frequency.

Uses of Function Generators in Everyday Applications

Despite the heavy association of function generators with specialized fields like electronics engineering and research, their applications aren't solely confined to these domains. Indeed, function generators are used in a range of everyday applications that impact our lives more directly than we may realize.

Telecommunications: Modern communication systems are underpinned by signal transmission and processing principles. Function generators are essential in designing, testing, and troubleshooting these systems, making them vital to our digital, interconnected world.

Automotive Electronics: In the automotive industry, function generators are used for testing electronic control units (ECUs), radios, and infotainment systems. They also play a role in designing and testing sensors, ensuring the smooth functioning of features like parking assistance and automated braking.

Medical Equipment Testing: Medical devices like heart rate monitors and imaging systems rely on electronic signals for operation. Function generators are crucial for testing these devices, ensuring accuracy and reliability in the healthcare field.

Audio Systems: In the realm of audio systems, function generators are used to create audio frequencies for testing speakers, microphones, and other audio equipment, contributing to the quality of sound that we enjoy in our daily lives.

These applications demonstrate that function generators contribute significantly to the functionality and reliability of many devices we rely on daily.

Types of Function Generators

Function generators come in various types, each offering unique advantages. Here's a brief look at some common types:

  • Analog Function Generators: These are conventional function generators. They can produce sine, square, and triangular waveforms.
  • Digital Function Generators: These function generators use digital technology to generate signals. They offer greater stability and precision compared to their analog counterparts.
  • Arbitrary Waveform Generators (AWGs): AWGs are high-end function generators capable of generating any waveform that can be described mathematically.
  • Software Function Generators: These are software-based tools that generate waveforms. They are typically cost-effective and can be a viable alternative for applications that do not require high precision.
  • RF and Microwave Signal Generators: These generators are used when a higher frequency range is required.
     

Choosing the Right Function Generator

Choosing the right function generator can be a daunting task, given the variety of available options. Some key factors to consider while selecting a function generator are:

  • Frequency Range
  • Waveform Types
  • Accuracy and Stability
  • Amplitude Range
  • Modulation Types
  • Ease of Use

Consider these factors in line with your unique requirements to choose the right function generator for your application.

Comparing Function Generators

Type Waveforms Frequency Range Modulation Use Case
Analog Function Generators Sine, Square, Triangle Limited range, typically up to 20MHz Limited modulation types General-purpose, low-cost applications
Digital Function Generators Sine, Square, Triangle, Pulse Higher than Analog, typically up to 120MHz More modulation types More precise applications
Arbitrary Waveform Generators (AWGs) Any mathematically described Similar to digital generators, sometimes higher More modulation types High-end applications requiring custom waveforms
Software Function Generators Depends on the software Typically lower Depends on the software Applications that do not require high precision
RF and Microwave Signal Generators Typically sine Very high, typically into GHz More modulation types Applications requiring very high frequencies

Key Takeaways

Function generators, with their ability to produce diverse waveforms at varying frequencies, play a critical role in testing, troubleshooting, and simulation within electronics. The variety in types – analog, digital, arbitrary waveform generators (AWGs), software, and RF and microwave signal generators – provide options tailored to specific requirements. 

When selecting a function generator, it is important to consider factors like frequency range, waveform types, accuracy, and stability, to harness the full potential of these indispensable tools in electronic engineering.

Keysight Signal Generators and Waveform Generators

Buying a used signal generator or waveform generator is the best way to save money without sacrificing quality. You can save up to 90% when purchasing from Keysight Technologies!

We offer a wide range of high-quality, premium, refurbished signal generators and waveform generators backed by a 1-year warranty. You can be confident you are choosing a quality oscilloscope supported by a trusted manufacturer.

Check out our premium Used Equipment page to choose a premium refurbished oscilloscope with some of the highest standards and specifications in the industry.

Browse Signal, Function + Waveform Generators at a Great Discount

すべてを見る Signal Generators
  • Like-new Condition
  • Updated Firmware
  • Full Calibration
  • New Accessories
  • Like-new Warranty
  • Customization possible

Learn more

  • Savings of up to 90%
  • Working Condition
  • Calibrated or Tested
  • 30-Day Right-of-Return
  • No Customization
  • Shipping to limited countries

Learn more

Select up to 3 instruments to compare

Cancel
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at
Select another instrument to compare
Starting at

Whenever You’re Ready, Here Are
5 Ways We Can Help You

1

Browse our Premium Used Equipment.

2

Call tech support US: +1 800 829-4444
Press #, then 2. Hours: 7am – 5pm MT, Mon– Fri

3

Contact our sales support team

4

Create an account to get price alerts and access to exclusive waitlists

5

Talk to your account manager about your specific needs

Callum Reed
Used Equipment Store Marketing Manager
ご意見・ご感想をお寄せください
Stay Up to Date on Used Equipment!

Don’t miss special offers, news, and announcements on the latest used equipment. Unsubscribe at any time.

Get Email Updates