백서
Organizations today face a host of challenges to remain competitive. Their core goal is they want high quality products and services with faster time to market. To achieve that, they must test thoroughly and with effective repeatability. What makes it challenging is that manual testing is time consuming, lab equipment is expensive, while budgets and testing skills are straining. The solution is to be able to increase equipment utilization and automate, an in turn accelerate, everything in the testing process. But testing faster can’t allow a compromise in quality. Not all automation solutions in this space are the same. How organizations approach the objective of ensuring speed and quality in testing is a critical challenge. One essential component of an effective test automation and lab operations solution is the caliber of the REST APIs (representation state transfer application interface) provided as components in the solution. They can represent a make-or-break factor in a solution’s value and capability to support the organization’s goals of optimal test automation and lab operations. This white paper examines the evolution of REST APIs, provides insight into the state-of-the-art of REST APIs, how they support continuous testing objectives in DevOps, and how they foster comprehensive automatability in testing.
무엇을 찾고 있습니까?