アプリケーションノート
Ethernet is fast emerging as that single shared medium as recent technology developments make Ethernet viable for use in cars. The Ethernet used in automobiles has different electrical requirements (EMI/RFI emissions and susceptibility), and is known as Automotive Ethernet. Automotive Ethernet is not only for the “luxury” car market trends indicate that a significant majority of car manufacturers are planning to move to Ethernet for all classes of cars.
This Black Book includes functionality, pentesting, and impairment methodologies that can be used to verify device and system functionality and performance. The methodologies are universally applicable to any test equipment. Step-by-step implementation examples using Ixia's test platforms and applications are included to demonstrate the art of the possible.
何をお探しですか?