Meet Signal Integrity Challenges in Complex Medical Systems

Notas de Aplicação

High-Speed Digital Technology Enables Exciting Advances in Complex Medical Systems

The tremendous growth in both the number of complex medical systems and the increasing capabilities of those systems is enabling previously unimaginable applications. Medical imaging systems are enabling early detection of health conditions in orthopedics, obstetrics, gynecology, nephrology, neurology, cardiology, pulmonology, and more. Surgical robots, hospital facilities robots, and telehealth systems are helping medical practitioners detect and diagnose medical conditions and enhance care in ways that extend the lives of millions of patients. As we will see, all these capabilities are enabled by high-speed digital signals, which means that the signal integrity in these systems is more important than ever.