IxNetwork MCP

Datenblätter.

IxNetwork MCP is a Model Context Protocol (MCP) server that connects IxNetwork to AI agents and LLM-based tools, letting network test engineers drive test configuration, execution, and analysis through natural-language, AI-assisted workflows — without abandoning existing scripts, REST API integrations, or GUI workflows.

 

Install / connect the IxNetwork MCP server to an existing IxNetwork instance. Point an MCP-compatible AI client (for example, Claude Code, an internal agent) at the IxNetwork MCP server. Describe test intent in natural language — the AI agent calls IxNetwork MCP tools to configure and run the test. Review results, statistics, and exported configs as usual.

 

See here for more information on IxNetwork.