Why Teams Choose Keysight Eggplant Test

Most test automation was built for simple systems and web browsers. As applications grow more connected, more regulated, and more critical to enterprises, script-first approaches start to fail.

Tests become fragile. Maintenance grows. Confidence drops just when it matters most.

Keysight Eggplant Test was designed for the real world.

Instead of scripting isolated checks, teams model real user journeys and validate behavior from the user's point of view.

That means testing complete workflows across UIs, APIs, and complex systems, not just what's easy to automate.

See Keysight Eggplant Test in Action

Test real user journeys, not just scripts.

Keysight Eggplant Test allows you to model how applications are actually used, then automatically explores and validates complete workflows across UI, APIs, and complex systems.

Teams find issues earlier, reduce maintenance, and make release decisions based on evidence, not assumptiosn.

Outcomes Teams Acheive with Keysight Eggplant Test

Tick box

Faster Time to Value

Speed up testing cycles with AI-driven automation, so teams can deliver quality software quickly.

quality

Detect Issues Early

Catch issues early with intelligent automated testing that improves accuracy and reduces risk.

Brain

Cover Every User Journey

Ensure every interaction, integration and workflow is tested across all platforms and environments.

Brain

Test the Complex

Automate load testing across complex systems from web and mobile to API and secured systems such as Citrix.

Trusted by teams who test smarter and release faster

AI Jumpstart

Generate Test Assets Directly from Requirements

Keysight Generator uses Gen AI to transform requirements into high-quality test assets. These assets reduce test asset creation by up to 70%, helping teams start testing easlier and reduce manual creation.

From aerospace and defense to retail, Generator supports compliance, scales coverage, and frees teams from repetitive test writing, allowing them to focus on innovation.

Resources to get you started

Explore Keysight's software testing best practices guides, trend reports, eBooks, and more.

Front Cover of The Utlimate AI Testing Playbook

The Ultimate AI Testing Playbook

The pressure to release updates faster is greater today than ever to keep up with customer expectations. DevOps and continuous testing should provide the answer to keeping up with the pace of change, but unless testing teams harness everything these ways of working have to offer, they aren’t enough.

As this playbook explains, the key to success is adding AI testing to the toolkit.

 

 

모든 리소스 보기

Frequently asked questions about Keysight Eggplant Test

Keysight Eggplant Test is an AI-powered test automation platform that enables teams to perform end-to-end software testing, automate user journeys, and deliver high-quality applications faster.

Keysight Eggplant Test uses AI-driven test generation and execution to increase test coverage, detect defects earlier, and ensure more reliable releases. This reduces your risk while improving overall software quality.

Common types of software testing include manual testing, automated testing, functional testing, non-functional testing (like performance and security testing), unit testing, integration testing, system testing, and acceptance testing.

Black box software testing is an approach where the tester assesses the software’s functionality without any knowledge of the application’s internal workings. In contrast, white box testing involves a thorough examination of the internal logic and structure of the code, requiring full visibility of the source code.

Deciding between manual testing and software test automation depends on various project-specific factors, including requirements, timeline, budget, and testing scope. Manual testing is more suitable for exploratory, usability, and ad hoc testing, while automation is ideal for scenarios that require repetitive execution, such as automated regression testing.

Try Keysight Eggplant Test Today!

Get in touch for a demo or free trial of Keysight Eggplant Test.

Want Help or Have Questions?