Data Sheets
Faster Measurement Speed and Greater Measurement Accuracy
Skip the complicated setup and go straight to making measurements with the 8990B peak power analyzer from Keysight Technologies, Inc.This instrument offers faster measurement speed and greater measurement accuracy in key applications such as radar pulse analysis and wireless pulse measurement.Designed with both ease of use and high performance in mind, the 8990B peak power analyzer does more than just measure and analyze – it saves you time and effort, letting you focus on the important details.
8990B Peak Power Analyzer Key Features
–Capture short radar pulses accurately with a 5 nanosecond overall rise time/fall time – the fastest rise time/fall time in the peak power measurement market – when the 8990B peak power analyzer is paired with the either the N1923A or N1924A wideband power sensor.
Graphical User Interface Overview
Measurement screen
The main measurement screen is capable of displaying up to four traces: two RF traces, and two video traces (the triggering signal).Results are shown in the panel directly under the graphical window, with measurements displayed in the same color as the channel to which it corresponds.When a USB sensor is connected, the results for this additional channel can be overlaid on the same graphical window in compact mode, The main screen also features a soft panel key to the side of the graphical window, which lists the 15 pulse characterization measurements for quick measurement analysis.Users can select these measurement parameters via the touchscreen display, or by using the mouse.
Delay measurement
Perform delay measurements by pressing the Delay Measurement button on the soft panel key and two vertical markers will automatically detect the first pulse of the traces.The time delay between the two traces will be displayed in the measurement panel below the graphical window.
Droop measurement
The 8990B is the first peak power analyzer on the market to offer automated Pulse Droop measurement, which measures the amplitude degradation of the pulse top.This eliminates the need to manually manipulate the horizontal markers to make this measurement.Access the Pulse Droop measurement via the soft panel key.
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.