Choose a country or area to see content specific to your location
Application Notes
When debugging digital designs, it is often difficult-to-impossible to set up an oscilloscope to trigger on specific and unique signal problems. The Keysight Technologies, Inc. Zone Trigger, which is available as a standard feature in all InfiniiVision 3000T, 4000 and 6000 X-Series oscilloscopes, can be used in conjunction with conventional oscilloscope triggering to help zero-in on problem signals. If you can see the problem signal, then you can trigger on it using Zone Trigger.
The best way to understand what Zone Trigger can do for you is to see some examples. This application note will show the following four measurement applications:
Unlock Content
Sign up for free
*Indicates required field
Thank you.
Your form has been successfully submitted.