Adobe Flash Player MovieClip Method Call Use After Free

Strike ID:
E16-69j01
CVSS:
9.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
2
Year:
2016

Description

This strike exploits a remote code execution vulnerability in Adobe Flash Player. The vulnerability is due to a use after free in call methods on a MovieClip. An attacker can entice a target to open a specially crafted flash file to trigger the vulnerability. Successful exploitation may result in execution of arbitrary code or abnormal termination of the flash process.

CVE

Google

Bid