Choose a country or area to see content specific to your location
eBooks
5G is a revolution, an evolution, and a reality. Naturally, when a technology like 5G is evolving, carriers and mobile operators face design spin ups to conform to the 3GPP standards. There is a need to properly understand the potential of 5G in the Internet of Things (IoT) and telecommunications, connected vehicles, and augmented and virtual reality (AR/VR) domains. Being first and best in 5G depends on how prepared you are.
5G For Dummies, Ixia Special Edition, consists of eight short chapters that explore:
5G for Dummies also provides a peek into the 5G networks of the future, various use-case scenarios, and the technologies that will be leveraged in the unlicensed spectrum.