D9010CAUC CAUI-4 Compliance Test Application Software

Datenblätter.

D9010CAUC CAUI-4 Compliance Test Application Software

The Keysight Technologies, Inc. D9010CAUC CAUI-4 compliance test application provides a fast and effortless way to test, debug and characterize your CAUI-4 designs. The tests performed by the D9010CAUC software are based on the IEEE 802.3 Specification. In addition, the application features tools for finding the optimal CTLE eye opening, TP4 Crosstalk Generator Amplitude Calibration and TP4 Crosstalk Transition Time Calibration. The test application offers a user-friendly setup wizard and a comprehensive report that includes margin analysis.

Transform complexity into simplicity

• Setup wizard for quick setup, configuration and test selection.

• Execution speed and proven test algorithm which minimizes test time.

• User-select tests and configuration based on the IEEE802.3 CAUI-4 specification.

• Team framework that reports multi trials with full array of statistics for each measurement with worst case measurement results.

• Accurate and repeatable results with Keysight Technologies Infiniium oscilloscopes

• Automated reporting in a comprehensive HTML format with margin analysis.

With the D9010CAUC CAUI-4 Ethernet electrical test software, you can use the same oscilloscope you use for everyday debugging to perform automated testing and margin analysis based on the IEEE802.3-2018 standard.

D9010CAUC Compliance Test Application Software Saves You Time

The D9010CAUC CAUI-4 Ethernet electrical compliance test application software saves you time by setting the stage for automatic execution of CAUI-4 electrical tests. Part of the difficulty of performing electrical tests for Ethernet transmitters is properly connecting to the oscilloscope, loading the proper setup files, and then analyzing the measured results by comparing them to limits published in the specification. The Ethernet electrical compliance test application software does much of this work for you. The CAUI-4 Ethernet electrical compliance test application software automatically configures the oscilloscope for each test, and it provides an informative results report that includes margin analysis indicating how close your product is to passing or failing that specification.

Easy test definition

The D9010CAUC CAUI-4 Ethernet electrical compliance test application software extends the ease-of use advantages of Keysight’s Infiniium oscilloscopes to testing CAUI-4 designs. The Keysight automated test engine walks you quickly through the steps required to define the tests you want to make, set up the tests, perform the tests, and view the test results. A setup page enables you to quickly make decisions from the outset regarding the choice of tests and perform functions that affect the testing task. The test selections available in the following steps are then filtered according to the choices made in the setup page. While selecting tests, you can select a category of tests all at once or specify individual tests. You can save tests and configurations as project files and recall them later for quick testing and review of previous test results. Straightforward menus let you perform tests with a minimum of mouse clicks.

Compliance measurement tests

The D9010CAUC CAUI-4 compliance test application allows you to run single or multiple tests based on your needs. Highlight a test to show more details including tests limits and references to related details of the specification. Accurate and repeatable results give you confidence in your measurements. You can also specify the number of test trials and only stop running selected tests when the stop condition is met. The application will save the worst-case test result to help you track down the anomalies in your signals.

Configurability and Guided Connection

The D9010CAUC CAUI-4 compliance test application provides flexibility in your test setup. The application lets you define controls for critical test parameters such as voltage threshold values, number of waveforms used for analysis and customizable violation settings. Once you have configured the tests, the connection page will display the connection diagram for the test you have selected. The compliance application guides you to make connection changes with hookup diagrams when the tests you select require it. You connect the oscilloscope to the device under test using Wilder test fixture www.wilder- tech.com. SMA cables may be required to attach the Wilder test fixtures to the Keysight Infiniium oscilloscope. See ordering information for more details.

Comprehensive Result Analysis

In addition to providing you with measurement results, the D9010CAUC CAUI-4 compliance test application software provides a report format that shows you not only where your product passes or fails, but also reports how close you are to the limits specified for a test. You can select the margin test report parameter, which means you can specify the level at which warnings are issued to alert you to electrical tests where your product is operating close to the official test limit defined by the CAUI-4 specification.

Thorough Performance Reporting

The D9010CAUC CAUI-4 compliance test application software generates HTML reports that captures the performance, status and margins of your device under test. It also captures screenshots of critical measurements of your reference and documentation. This report is suitable for printing and sharing with your test vendors, customers and suppliers.

Recommended Oscilloscope

The D9010CAUC CAUI-4 Compliance Test Application Software is compatible with Keysight Infiniium Series oscilloscopes with operating software revision 6.30 or higher.

Flexible Software Licensing and KeysightCare Software Support Subscriptions

Keysight offers a variety of flexible licensing options to fit your needs and budget. Choose your license term, license type, and KeysightCare software support subscription.

License terms

• Perpetual – Perpetual licenses can be used indefinitely.

• Subscription – Subscription licenses can be used through the term of the license only

(6, 12, 24, or 36 months)

License types

• Node-locked – License can be used on one specified instrument/computer.

• Transportable – License can be used on one instrument/computer at a time but may be transferred to another using Keysight Software Manager (internet connection required).

• USB Portable – License can be used on one instrument/computer at a time but may be transferred to another using a certified USB dongle (available for additional purchase with Keysight part number E8900-D10).

• Floating (single site) – Networked instruments/computers can access a license from a server one at a time. Multiple licenses can be purchased for concurrent usage.