Spectrum Analysis Amplitude and Frequency Modulation

Applikationsberichte

Chapter 1. Modulation Methods

Modulation is the act of translating some low-frequency or baseband signal (voice, music, and data) to a higher frequency. Why do we modulate signals? There are at least two reasons: to allow the simultaneous transmission of two or more baseband signals by translating them to different frequencies, and to take advantage of the greater efficiency and smaller size of higher-frequency antennae. In the modulation process, some characteristic of a high-frequency sinusoidal carrier is changed in direct proportion to the instantaneous amplitude of the baseband signal. The carrier itself can be described by the equation.

e = A cos (ωt + φ)

where:

  • A = peak amplitude of the carrier,
  • ω = angular frequency of the carrier in radians per second,
  • t = time, and
  • φ = initial phase of the carrier at time t = 0.

In the expression above, there are two properties of the carrier that can be changed, the amplitude (A) and the angular position (argument of the cosine function). Thus we have amplitude modulation and angle modulation. Angle modulation can be further

characterized as either frequency modulation or phase modulation.