Technische Überblicke
Keysight Technologies
Mobile WiMAX™ X-Series Measurement App, Traditional UI N9075EM0D
Technical Overview
– Mobile WiMAXTM RF transmitter measurements
– Single-channel matrix A modulation analysis and pilot-based matrix B (wave 2) analysis
– One-button tests with pass/fail limits per Mobile WiMAX standard
– Hardkey/softkey manual user interface and SCPI remote user interface
– Built-in context sensitive help
– Flexible licensing provides the option of using perpetual or time-based licenses with one or multiple signal analyzers
Mobile WiMAX Measurement Application
The Mobile WiMAX measurement application transforms the X-Series signal analyzers into standard-based Mobile WiMAX transmitter testers by adding fast one-button power and modulation measurements to help you design, evaluate, and manufacture your Mobile WiMAX devices, based on IEEE 802.16e-2005 and WiBro. When the Keysight Technologies, Inc. N9030A PXA or N9020A MXA signal analyzer has optional baseband IQ inputs, Option BBA, each of the RF and analog baseband IQ signals of Mobile WiMAX can be measured to compare signal quality.
X-Series measurement applications can help you:
– Gain more insight into device performance with intuitive display and graphs for your application. Select from our library of over 25 different measurement applications.
– Ensure that your design meets the latest standard. Updates are made to the X-Series measurement applications as standards evolve.
– Apply the same measurement science across multiple hardware platforms for consistent measurement results over your design cycle from R&D to production.
– Choose the license structure that meets your business needs. We provide a range of license types (node-locked, transportable, floating or USB portable) and license terms (perpetual or time-based).
Mobile WiMAX Overview
The IEEE 802.16e-2005 standard, often referred to as Mobile WiMAX, defines the physical layer (PHY) and medium access control (MAC) protocol for products that extend broadband wireless access (BWA) from the local area network (LAN) to the metropolitan area network (MAN). The standard contains specifications for licensed and unlicensed BWA operating between 2 and 11 GHz. The term OFDMA used to describe this new technology means orthogonal frequency division multiple access and it distinguishes the system from OFDM technologies such as Fixed WiMAX or 802.11 WLAN. The standard includes an OFDMA PHY layer with sub-channelization that allows the time and frequency resources to be dynamically allocated among multiple users across the downlink (DL) and uplink (UL) sub-frames. It uses a combination of TDD and OFDMA for downlink and uplink signaling and multiple user access. The unique features within the TDD/ OFDMA frame provide frequency diversity, frequency reuse, and cell segmentation which improve the performance against fading and inter-cell interference.
For data transmission the standard defines a set of adaptive modulation and coding rate configurations that can be used to trade off data rate for system robustness under various wireless propagation and interference conbits/symbol) that will result in more system capacity. When link conditions are poor due to problems such as signal fading or interference, the WiMAX system can change to a lower modulation scheme to maintain an acceptable radio link margin. The allowed modulation types are binary phase shift keying (BPSK), quadrature phase shift keying (QPSK), 16 quadrature amplitude modulation (16QAM), and 64QAM.
The WiMAX ForumTM is comprised of industry experts whose charter is to bring the IEEE 802.16 standard to the marketplace and to create the process for certification and inter-operability between equipment vendors. The WiMAX Forum tests operational performance based on the standard through the use of radio and protocol conformance test documentation. Subsets of system features are known as profiles, which specify the mandatory and optional features from the 802.16 standard required for baseline functionality and interoperability. The choice of profiles has been driven by spectrum availability, regulatory constraints, and market demand. The WiMAX Forum specifies a series of protocol and radio conformance tests (RCT) for compliance and interoperability between various equipment manufacturers. Certification test houses, such as AT4 Wireless in Spain and Telecommunications Technology Association (TTA) in Korea, were among the first to be approved by the WiMAX Forum to provide conformance testing to the WiMAX profile specifications.
In order to support increased range, link reliability, and throughput, several advanced features are supported in wave 2. These include DL/UL adaptive modulation and coding (DL/UL AMC zones), beamforming, space time coding (STC) or matrix A, 2x2 MIMO with vertical encoding or matrix B, and collaborative spatial multiplexing uplink (CSM). The use of 2 antennas for transmission and 1 for reception gives the notation 2x1, and the use of 2 antennas for transmission and 2 for reception gives the notation 2x2. Matrix A and matrix B zones may be transmitted by a base station with two transmit antennas. In the downlink subframe, the preamble is followed by the first zone–a mandatory PUSC zone that contains the FCH, the DL-MAP, and the ULMAP. The preamble and first zone are transmitted only by antenna 0. Antenna 1 is generally expected to be inactive during this time, but becomes active with the first matrix A or matrix B zone in the subframe.
Können wir Ihnen behilflich sein?