E5080A ENA: Code Compatibility Solutions for E5071C and 8753 Network Analyzer Users

Flyer

Keysight Technologies

E5080A ENA: Code Compatibility Solutions for E5071C and 8753 Network Analyzer Users

Introduction

The Keysight Technologies, Inc. E5080A ENA network analyzer offers the compatibility solutions that help you migrate your E5071C and 8753 network analyzers to the E5080A. The compatibility solutions support the majority of commands and functions used in the S-parameter measurements. You can seamlessly migrate your automatic test equipment (ATE) systems to next generation with minimal efforts, and take advantage of improved performance and measurement speed using the E5080A. 

E5071C Code Emulation and State File Conversion Tools

The E5071C compatibility solution consists of two elements—the E5071C code emulation mode and the E5071C state file converter. 

E5071C Code Emulation mode

The E5071C Code Emulation mode enables the E5080A to run remote programming codes with E5071C SCPI commands. The command emulation is performed by the firmware in real time. You can start the emulation mode by choosing “5071” in the Code Emulation softkey under the System menu

E5071C state file converter

The state file compatibility is also important because many manufacturing customers save their test settings in the state files. The E5071C state file converter is the application software that converts the E5071C’s state files to the E5080A’s. The state file conversion between two analyzers can be easily done by using a USB memory stick.

8753 Code Emulation Tool

The 8753 Code Translator (CxL) is the application software which runs on the E5080A and emulates the 8753 commands