Test Exec SL 6.1 Basics Training

Datenblätter.

Course Overview

This course gives an in-depth introduction into the us­age of the test sequencer Test Exec SL and provides an overview of the different automotive test system solutions of the Keysight Technologies, Inc. TS-5400 family. The attendee will learn how to use the different features of the Test Exec SL software. An important aspect is the capa­bility to design a functional test solution which reflects the requirements of a customer specific test application. The course develops step by step the theoretical basics and provides comprehensive hands on labs to verify and consolidate the knowledge.

Technical Overview - Detailed Course Agenda

Primary target is to understand and to use the test execu­tive software development platform in order to quickly develop reusable automated functional tests. Attendees will explore details of the Test Exec SL test sequencer and adapt the software configuration, system topology and test description according to the lab setup composed out of a set of core instruments. Central element of this lab setup is the 34980A switch measure unit with its internal digital multi meter and the 34933A matrix card as well as the 33220A Arbitrary Waveform generator and the MSO6054A Oscilloscope. Basic capabilities of the used instruments and useful hardware and software tools are introduced in order to enhance the hands on experience