How to Generate and Simulate a Dynamic Gain Model in PathWave Advanced Design System (ADS)

Applikationsberichte

This application note explains and illustrates how to generate a dynamic gain (DG) model from a circuit envelope (CE) simulation of a power amplifier (PA) schematic in the PathWave Advanced Design System (ADS). The extracted DG model is reused and re-simulated in a CE test bench in the second section. The dynamic gain model was developed at Keysight to model very long memory effects 1.