Keysight Launches Wireless Test Platform for Wi-Fi 7 

  • Turnkey solution simulates Wi-Fi devices and traffic to cover new use cases on the latest IEEE 802.11be standards
  • Delivers signaling radio frequency and throughput testing at Wi-Fi 7 scale including 4X4 MIMO 320 MHz bandwidth
  • Combines capabilities for faster test setups, less complexity, and better performance to accelerate time-to-market for Wi-Fi 7 devices

SANTA ROSA, Calif. February 13, 2024  

Keysight Technologies, Inc. (NYSE: KEYS) introduces the E7515W UXM Wireless Connectivity Test Platform for Wi-Fi®, a network emulation solution delivering signaling radio frequency (RF) and throughput testing for devices using Wi-Fi 7, including 4x4 MIMO 320 MHz bandwidth. 

Developed by the IEEE as the 802.11be standard, Wi-Fi 7 is the next generation of Wi-Fi wireless communications technology, promising significant performance advancements and improvements over the previous Wi-Fi 6E and Wi-Fi 6 standards. As with any new wireless technology, device makers must perform extensive signaling RF and throughput on clients and access points (AP) to ensure Wi-Fi 7 devices work as intended when deployed. However, existing solutions require extremely complicated test setups with large number of Wi-Fi devices and network channels to emulate real-world operating conditions.

The newest Keysight UXM Wireless Connectivity Test Solution addresses this challenge by giving RF engineers a turnkey solution that simplifies Wi-Fi 7 testing and provides unique physical (PHY) layer and media access control (MAC) layer insights.

The E7515W UXM Wireless Connectivity Test solution offers the following benefits:

  • Built on proven Keysight metrology: Expands the market leading UXM 5G Network Emulation Solution to simulate Wi-Fi devices and traffic to cover new use cases on the latest IEEE 802.11be standards.
  • Wi-Fi 7 scale: Emulates hundreds of clients at once – three-times more than existing solutions in the market – with traffic simulation without the need for additional equipment.
  • Wi-Fi 7 throughput: Supports Wi-Fi 7 4x4 MIMO 320 MHz bandwidth and performs Wi-Fi 7 signaling RF and throughput testing on clients and APs, including the latest 802.11 variants.
  • Deeper insights: Uses analysis software to provide PHY / MAC-level information such as rate versus range, enhanced Rx sensitivity, radio unit (RU) sweep analysis, and full-rate throughput to generate relevant Wi-Fi signaling and RF throughput results.
  • Integrated, turnkey platform: Tests more complex devices with 5G and LTE capabilities Wi-Fi / cellular interworking validation as well as integrated fixed wireless access (FWA) testing for the fast-growing customer premises equipment (CPE) market.
  • Simplified testing: Offers inherent synchronization, better repeatability, reduced time spent on cabling and test setup, higher automation, and faster debugging and reporting.

Mosaab Abughalib, Senior R&D Director and General Manager for Keysight's Wireless Test Group, said: "With the introduction of the E7515W solution, Keysight is expanding the market leading UXM 5G Network Emulation Solutions to simulate Wi-Fi devices and traffic to cover new use cases from the latest IEEE 802.11be standards. The E7515W solution enables faster test setups with less complexity and delivers better load and bandwidth performance to help Wi-Fi 7 device makers accelerate time to market."

Resources

About Keysight Technologies   

At Keysight (NYSE: KEYS), we inspire and empower innovators to bring world-changing technologies to life. As an S&P 500 company, we're delivering market-leading design, emulation, and test solutions to help engineers develop and deploy faster, with less risk, throughout the entire product lifecycle. We're a global innovation partner enabling customers in communications, industrial automation, aerospace and defense, automotive, semiconductor, and general electronics markets to accelerate innovation to connect and secure the world. Learn more at Keysight Newsroom and www.keysight.com

Keysight Contact:

Paul Erwin, Americas
+1 248 430–9075
paul.erwin@keysight.com

Fusako Dohi, Asia 
+81 42 660–2162
fusako_dohi@keysight.com

Jenny Gallacher, Europe
+44 (0) 7800 737–982
jenny.gallacher@keysight.com 

Keysight introduces the E7515W UXM Wireless Connectivity Test Platform for Wi-Fi®, a network emulation solution delivering signaling radio frequency and throughput testing for devices using Wi-Fi 7.