How to Reduce Power-Line Noise in DC Measurements

Advanced Benchtop Digital Multimeter
+ Advanced Benchtop Digital Multimeter

Prevent Power-Line Noise from Distorting DC Readings

Precision DC measurements can become difficult to trust when 50/60 Hz power-line interference couples into the signal path and adds periodic variation to otherwise stable readings. The effect can be especially noticeable when engineers are measuring small DC changes, comparing repeated results, or validating circuits where only a narrow margin separates expected behavior from a possible fault. As line-frequency noise appears in the measured value, readings may fluctuate enough to obscure real device changes, complicate trend comparisons, and make it harder to determine whether variation comes from the device under test or from the surrounding bench environment. These problems can extend validation time because engineers may need to repeat measurements, adjust the setup, or investigate apparent changes that are actually caused by external electrical interference.

The impact of power-line noise also depends on how the measurement is acquired. When the measurement aperture is not aligned with the local power-line cycle, unwanted 50/60 Hz content can pass into the reported DC value instead of averaging toward zero. This can reduce normal-mode rejection and increase reading variation, especially when small differences matter. Engineers need to understand how integration time, line frequency, and measurement speed interact before deciding whether a changing result reflects true circuit behavior. Faster acquisition settings can reduce noise rejection, while conservative settings can slow testing unnecessarily. Balancing these factors helps engineers obtain repeatable DC measurements during system validation, characterization, troubleshooting, and other bench workflows where measurement confidence is critical.

Power-Line Noise Rejection Solution

Reducing power-line interference begins with configuring the measurement so 50/60 Hz noise is rejected before it distorts the reported DC value. Keysight Advanced Benchtop Digital Multimeters support this workflow with selectable Number of Power Line Cycles (NPLC) integration settings and normal-mode rejection capabilities that let engineers balance measurement speed, resolution, and noise performance for the task at hand. Using integration times aligned to whole power-line cycles helps suppress line-frequency interference and produce more repeatable DC readings, while longer integration settings can provide stronger noise rejection when maximum precision is more important than throughput. This approach helps engineers compare repeated measurements with greater confidence, identify small changes that are more likely to reflect actual device behavior, and avoid spending time troubleshooting noise introduced by the bench environment. The result is a more controlled precision DC measurement workflow that supports reliable validation, characterization, and debugging across a range of low-level electrical measurements.

See Block Diagram of Power-Line Noise Rejection Solution

Block Diagram of Power-Line Noise Rejection Solution

Explore Products for Our Power-Line Noise Rejection Solution

Discover Resources and Insights

Additional resources for Power-Line Noise Rejection

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?