How to Validate Receiver Across Cable Lengths

Receiver Test Solution
+ Receiver Test Solution

Measure Receiver Behavior By Cable Length

Validate receiver performance by repeating the same stressed test conditions over controlled automotive Ethernet cable lengths. Engineers configure representative cable assemblies, maintain the same receiver operating mode and test pattern, and record post-processing error results for each channel. The measurement can cover multiple data rates and channel constructions so that changes in loss and propagation conditions can be correlated with receiver behavior. Receiver BER validation is performed using a controlled channel and a repeatable measurement interval rather than changing several variables at once.

A systematic cable-length sweep can progress from shorter links to longer configurations while preserving the measurement sequence. Example channel evaluations may include 1 m, 12 m, and 15 m cable lengths with no observed post-FEC errors under the test conditions, followed by a 22 m configuration that produces more than 50 frame errors at 10 Gb/s as reported by the PHY ErrorCounter register. Engineers can use the same style of measurement to identify where receiver margin changes with channel length, compare supported data rates, and separate normal operating variation from a channel condition that exceeds receiver correction capability.

Cable Length Receiver Validation Solution

Perform the test by configuring repeatable cable assemblies at defined lengths and applying the same stressed receiver condition at each point in the sequence. The receiver test solution provides automated BER testing and measurement control for comparing receiver behavior across channel configurations. Engineers can log error-counter results for each cable length and data rate, then compare the results to identify channel-dependent changes in receiver margin. The workflow is useful for structured receiver BER validation because the physical channel becomes the primary variable while the receiver mode, stimulus, timing, and measurement procedure remain consistent.

See Block Diagram of Cable Length Receiver Validation Solution

Cable Length Receiver Validation Solution

Explore Products in Our Cable Length Receiver Validation Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?