How to Transfer Frequency Sweep Lists Using APIs

Expert Analog Signal Generator
+ Expert Analog Signal Generator

Transfer and Verify Frequency Sweep Lists

Frequency sweep list transfer begins by establishing a communication session between a host computer and a signal generator through a supported interface. The setup includes the instrument, a host application, the appropriate communication libraries, and a local area network (LAN), Universal Serial Bus (USB), or General Purpose Interface Bus (GPIB) connection. An application programming interface (API) provides functions for discovering the instrument, opening a session, and exchanging data. Engineers can use C or Component Object Model (COM) libraries to prepare a sequence of sweep-list entries and send it to the connected instrument. The example workflow uses a structured list of frequency and associated configuration values. Instrument-specific command syntax and the interpretation of list fields must be checked against the corresponding programmer’s manual before applying the sequence to a particular device.

After establishing the connection, the host application transfers the sweep list as a block of data and requests confirmation of the number of points received. It can then retrieve the processed list and compare the returned values with the original configuration. This readback step checks the integrity of the frequency sweep list transfer without assuming that the instrument has executed a physical sweep or produced measurement results. A repeatable workflow separates list preparation, transfer, point-count verification, readback, and session cleanup into distinct operations. Communication timeout settings and return codes help identify transport failures or incomplete exchanges. Binary block-transfer functions handle the data payload, while the host software parses the returned content and checks the expected structure. The instrument's programmer’s manual remains the authority for supported list formats, operating modes, and configuration parameters.

Frequency Sweep List Transfer Solution

Transferring a frequency sweep list requires a host application, a supported instrument connection, and software functions for sending and retrieving structured configuration data. Keysight C and Component Object Model (COM) communication libraries provide application programming interfaces (APIs) for local area network (LAN), Universal Serial Bus (USB), and General Purpose Interface Bus (GPIB) connections. These libraries enable instrument discovery, session management, frequency sweep list transfer, point-count verification, and readback of transferred configuration data. Engineers can integrate these capabilities into automated radio frequency (RF) testing applications to prepare frequency sweep configurations, transfer predefined settings to the signal generator, and verify that the instrument received the expected data. The Keysight Expert Analog Signal Generator can be incorporated into a software-controlled test environment, allowing engineers to manage instrument communication and streamline repetitive configuration tasks. Communication timeout controls, error reporting, and connection management functions support troubleshooting and consistent operation across repeated test sequences. Instrument-specific configuration capabilities and supported data formats are defined in the corresponding programmer’s manual.

See Block Diagram of Frequency Sweep List Transfer Solution

How to Transfer Frequency Sweep Lists Using APIs Block Diagram

Explore Products in Our Frequency Sweep List Transfer Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?