How to Measure RF Power Without a Separate Power Meter

USB Power Sensors
+ USB Power Sensors

Direct USB Power Measurements

Measuring radio frequency (RF) power typically requires a sensor to detect the applied signal and measurement electronics to convert the detected response into an average power result. A USB power sensor combines these functions in a compact measurement device that connects directly to a computer or compatible instrument, eliminating the need for a separate power meter. Engineers can connect the sensor directly to the radio frequency measurement point and use the USB interface for power, communication, configuration, and measurement acquisition. This reduces the number of instruments and interconnections required for development, functional verification, troubleshooting, and automated test workflows.

The measurement setup typically includes the radio frequency source or device under test, a USB power sensor, and a computer or compatible Keysight instrument. Engineers verify that the expected frequency and signal level fall within the sensor's supported measurement range, establish the appropriate radio frequency connection, perform zeroing as required, and configure the measurement. Average power readings can then be displayed and analyzed through supported software or retrieved programmatically for automated measurements. Direct USB connectivity provides a straightforward measurement path from the radio frequency test point to the host system while eliminating the conventional sensor-and-meter configuration.

Direct USB RF Power Measurement Solution

Direct USB power measurement integrates signal detection, measurement processing, instrument communication, and power delivery through a sensor connected to the host computer. Engineers connect the radio frequency signal to the sensor, establish USB communication, perform internal zeroing, and configure measurement parameters through supported software. BenchVue power meter and sensor software provides computer-based instrument control, measurement visualization, and data logging without requiring a separate hardware power meter. For automated test applications, the sensor can also be controlled programmatically and incorporated into repeatable acquisition sequences. Internal and external triggering extend the workflow to measurements requiring defined acquisition timing, while trace display can provide a graphical view of the signal envelope for trigger and gate setup. Compatibility with other Keysight instruments allows the same USB sensor architecture to be incorporated into broader radio frequency test configurations. This direct-connect approach reduces bench hardware while supporting interactive, automated, and instrument-integrated average power measurement workflows.

See Block Diagram of Direct USB RF Power Measurement Solution

Block Diagram of Direct USB RF Power Measurement Solution

Explore Products in Our Direct USB RF Power Measurement Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?