How to Measure Capacitance and IV

Parameter Analyzer
+ Parameter Analyzer

Measure CV And IV Accurately

Discerning whether newly formed lithium-ion (Li-ion) battery cells in electric vehicles (EVs) exhibit acceptable self-discharge behavior requires a potentiostatic measurement method. A low-noise, very stable DC source is set to match the cell's open-circuit voltage (OCV). The DC source connects to the cell through a micro-ammeter and the current flowing between the DC source and the cell is measured. When the cell self-discharges, the DC source takes over, furnishing current to maintain the cell at a constant voltage and state of charge.

As the DC source comes to equilibrium with the cell, the self-discharge current transitions from internally sourced to furnished externally from the DC source. Self-discharge current is measured using the micro-ammeter. The potentiostatic measurement method requires a self-discharge analyzer capable of quickly matching the voltage to within +/- 5 µV of the cell’s OCV before being applied. This process minimizes the introduction of any new charge or discharge changes, limiting measurement settling time to a minimum. The voltage applied to the cell must also be stable to minimize ongoing current noise on the self-discharge current measurement.

Capacitance And IV Measurement Solution

Accurate capacitance-voltage and current-voltage testing requires correct four-terminal connections, a stable return path, and compensation for residual cable impedance and stray admittance. The solution combines a semiconductor device analyzer with source/measure and capacitance measurement capability, automated switching between CV and IV paths, and support for open, short, and load correction in shielded two-terminal setups. It helps configure measurements through a graphical application library, with graph or list results, while supporting capacitance measurement from 1 kHz to 5 MHz, automated return-path control, and on-wafer measurement workflows.

See Block Diagram of Capacitance And IV Measurement Solution

Block Diagram of Capacitance And IV Measurement Solution

Explore Products in Our Capacitance And IV Measurement Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?