How to Automate Multi-Channel Signal Generator Setup

Essential Analog Signal Generator
+ Essential Analog Signal Generator

Automate RF Channel Setup

Automating multi-channel signal generator setup requires remote commands to configure each radio frequency channel independently while preserving shared instrument settings. Engineers can set channel-specific frequency, power, modulation, and output state, then apply common reference or system settings as needed. This enables repeatable multi-channel stimulus without manual configuration for each test condition.

A controller connects to the signal generator through the supported remote interface and sends commands to selected channels. Each channel can have its own carrier and output state, while shared nodes control instrument-wide settings. This supports repeatable receiver stimulus, component characterization, phase-coherent source setup, and automated validation while reducing setup time and configuration errors.

Multi-Channel Setup Automation Solution

Automate multi-channel signal generator setup by programming each source and output channel through remote commands and applying shared instrument settings where required. The solution uses a Keysight Analog Signal Generator to configure multiple radio frequency channels from a single instrument. Engineers can automate frequency, power, modulation, and radio frequency output state per channel while managing common reference-related settings across the device. This enables repeatable multi-path receiver stimulus, component testing, phase-coherent source configuration, and automated test systems that require consistent channel-by-channel setup.

See Block Diagram of Multi-Channel Setup Automation Solution

How to Automate Multi-Channel Signal Generator Setup Block Diagram

Explore Products in Our Multi-Channel Setup Automation Solution

Discover Resources and Insights

Additional Resources for Multi-Channel Setup Automation

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?