Real Results Teams Acheive with Keysight Eggplant Test

Tick box

93% faster test execution

Reduce test cycles from 3 weeks to as little as 1 day

quality

3,730 testing days saved

Saving over $900k through automated regression testing

Brain

92% reduction in testing hours

Free teams to focus on innovation, not manual testing

Writing test cases by hand is the bottleneck nobody's fixed

Manual Test Case Creation

AI Test Case Generation with Keysight Eggplant

❌  Test case creation takes longer than testing the feature ✅  Automated test cases generated from your application model in minutes
❌  Scripts break the moment the UI changes ✅  Update the model once. Test cases rebuild themselves automatically
❌  Coverage stops where your imagination does
✅  AI covers every meaningful path, even ones you'd never consider 
❌  Regressions burns weeks before every release cycle ✅  Fujifilm cut 3 weeks of regression testing to 1 day
❌  More coverage means more manual work ✅  One model scales test coverage, so you focus on more valuable tasks

Request your demo

20 minutes. That's it. 

Bring one real test scenario and we'll show you AI test case generation working on your workflow.

Named a Leader in the 2025 Gartner® Magic Quadrant™ for AI-Augmented Software Testing Tools

Keysight is named a Leader in the 2025 Gartner® Magic Quadrant™ for AI-Augmented Software Testing Tools, reflecting Gartner’s evaluation of vendors based on Completeness of Vision and Ability to Execute.

Magic Quadrant for AI-Augmented Software Testing Tools

From One Journey to Scalable Coverage

Step 1. Model the journey

Define the wokflow, key states, and the variations that matter, such as user roles, business rules, data conditions, and environment differences.

Image showing how to build a model

Step 2. Generate paths from the model

ML algorithms and AI automatically derive executable paths to cover more meaningful journey combinations than manual scripting.

Model showing potential paths in an application

Step 3. Execute in real environments

Run across desktop, web, mobile, Citrix/VDI, and other restricted setups.

Keysight Eggplant running two factor authentication on Salesforce

Step 4. Review coverage and execution evidence

Review model coverage, executed paths, pass/fail outcomes, screenshots, logs, and run evidence to understand what was tested and what failed.

Report that shows bug hunting for Eggplant

Step 5. Update the model as workflows evolve

Update the model and reuse assets as the applications changes, without rebuilding large script suites.

Diagram showing how to edit and update a model

What Our Customers Say

AI Test Case Generation FAQs

Manual test case creation relies on a human thinking through every scenario, which means coverage is limited to what your team anticipates. AI test case generation derives paths from a model of how your application actually behaves, covering combinations and edge cases no manual process would catch. It also scales automatically when your application changes.

Yes. Keysight Eggplant uses image-based recognition rather than DOM hooks, so automated test cases run in any environment a human tester can see, including Citrix, VDI, remote desktops, and locked-down systems where most tools fail.

Most teams have a working application model and their first automated test cases executing within a day. You don't need to write scripts or instrument your app first.

Update the application model and test cases regenerate automatically. You're not rebuilding scripts, you're updating a model which is significantly faster and keeps your automated test case coverage current without manual rework.

Yes. Automated test cases can be triggered as part of your existing build pipeline. Keysight Eggplant integrates with standard CI/CD systems.