Eggplant for LMS testing automation, SIS validation, and EdTech accessibility testing across Canvas, Blackboard, Banner, Workday Student, and the integrations between them.
The pressure to release updates faster is greater today than ever to keep up with customer expectations. DevOps and continuous testing should provide the answer to keeping up with the pace of change, but unless testing teams harness everything these ways of working have to offer, they aren't enough.
As this playbook explains, the key to success is adding AI testing to the toolkit.
Topic Overviews
blogs
Solution Briefs
Eggplant tests and automates workflows across learning management systems (Canvas, Blackboard, D2L Brightspace, Moodle), student information systems (Banner, PeopleSoft, Workday Student, Jenzabar), online assessment platforms (Respondus, Honorlock, ExamSoft), library systems, and parent/student mobile applications. Most engagements focus on validating the integrations between these systems, where most institutional IT failures occur.
Yes. Because Eggplant tests at the UI level using image recognition, it validates legacy Banner and PeopleSoft interfaces with the same approach it uses for cloud-native Canvas or Workday Student. This makes it practical for higher-education IT environments where modernisation has been incremental and legacy systems run alongside SaaS replacements.
Eggplant validates accessibility by testing applications the way assistive technology experiences them; screen reader navigation, keyboard-only workflows, focus management, and dynamic content updates. This catches accessibility issues that static checkers miss, which is increasingly important under DOJ Title II rulemaking requiring state and local government entities (including public universities) to meet WCAG 2.1 AA standards.
Yes. A capability in Eggplant runs load testing for LMS, SIS, and assessment platforms. It simulates peak registration rushes, exam-week concurrent usage, and semester-transition loads, so capacity issues surface in test rather than during the peak itself.
Eggplant integrates with standard CI/CD platforms (Jenkins, GitLab, Azure DevOps) and connects with EdTech-specific procurement vehicles including state cooperative purchasing agreements. It is available through standard education sector IT procurement channels.
Most institutions see meaningful results within the first two quarters. Initial wins typically come from automating LMS regression testing through quarterly platform updates, validating peak registration readiness, or completing Section 508 audit cycles where manual accessibility testing was the longest-pole activity.
Können wir Ihnen behilflich sein?