Cisco_WebEx_Recording_Format_Player_atdl2006_dll_Buffer_Overflow_attack

Strike ID:
G12-41301
CVSS:
9.3 (AV:N/AC:M/Au:N/C:C/I:C/A:C)
False Positive:
f
Variants:
1
Year:
2012

Description

A code execution vulnerability exists in Cisco WebEx Recording Format (WRF) Player. This vulnerability is due to a buffer overflow when WRF player handles WRF files. A remote attacker can leverage this vulnerability by crafting a WRF file and enticing a target user to view the malicious file. Successful exploitation would result in execution of arbitrary code on the target host in the context of the application.

CVE

References

Bid