How to Measure Average Power of Frequency-Hopping Signals

Power Meters and Sensors
+ Power Meters and Sensors

Measure Frequency-Hopping Signal Power

Measuring average power in frequency-hopping radio frequency signals requires capturing signal energy across rapidly changing carrier frequencies while maintaining accurate time alignment and averaging. Frequency-hopping signals transition between discrete frequencies over defined intervals, which introduces challenges in ensuring that measurement systems capture all relevant signal energy without bias toward specific frequency states. Engineers must configure measurement systems that respond quickly to frequency changes while maintaining consistent averaging across the entire hopping sequence. Sensor bandwidth, response time, and measurement timing must be sufficient to track the signal behavior without introducing measurement gaps or distortion.

The measurement setup includes an average power meter, compatible wideband power sensors, and software capable of continuous acquisition and data logging. Engineers measure power across multiple hopping cycles to ensure that the resulting average represents the full frequency distribution of the signal. Proper averaging techniques and continuous measurement acquisition are required to capture variations between hops and ensure consistent results. Data analysis tools are used to verify measurement stability and confirm that all frequency states are included in the calculation, enabling accurate characterization of average power in frequency-hopping systems.

Frequency-Hopping Power Measurement Solution

Measuring average power of frequency-hopping radio frequency signals begins by configuring the power meter, sensor, and measurement software to continuously acquire power data throughout the entire hopping sequence. Engineers define acquisition duration, averaging behavior, sampling parameters, and logging intervals while the software manages uninterrupted measurements across successive hopping cycles. The solution combines an average power meter, USB and peak-and-average power sensors, and power measurement software to provide synchronized instrument control, continuous acquisition, automated averaging, real-time visualization, and long-duration data logging. Engineers can monitor average power across complete hopping patterns, compare multiple measurement runs, verify measurement consistency, and export results for documentation or additional analysis. Automated acquisition eliminates the need to manually synchronize measurements with individual frequency hops, providing a repeatable workflow for evaluating frequency-hopping transmitters during design validation, functional verification, production testing, and system performance characterization.

See Block Diagram of Frequency-Hopping Power Measurement Solution

N1913B Average Power Meter, BV0007B Power Meter Software, U2000A USB Power Sensor,  E9326A Peak and Average Power Sensor

Explore Products in Our Frequency-Hopping Power Measurement Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?