How to Automate RF Power Measurements Directly from a PC

USB Power Sensors
+ USB Power Sensors

Automate PC-Controlled Power Measurements

Automating radio frequency (RF) power measurements directly from a personal computer requires a measurement device that combines power sensing, measurement processing, and digital communication without relying on a separate hardware power meter. A USB power sensor provides this architecture by connecting the radio frequency signal directly to the sensor while using the USB interface for communication and power. Engineers can configure measurement parameters from the computer, acquire repeated average power readings, and integrate measurement results into automated validation or production workflows. Direct connectivity also reduces the number of instruments and interfaces required when building compact automated test configurations.

The measurement setup typically includes the radio frequency source or device under test, a USB power sensor, and a computer running supported measurement software or an automated test program. Engineers verify the expected frequency and signal level, establish the radio frequency connection, perform zeroing as required, and configure acquisition parameters before starting the measurement sequence. Repeated readings can then be collected programmatically, displayed for monitoring, or stored for subsequent analysis. Standard Commands for Programmable Instruments provide a consistent command interface for integrating power measurements into custom test applications and repeatable automated workflows.

PC-Controlled RF Power Measurement Solution

Direct computer control enables the USB power sensor to operate as a programmable measurement instrument within automated radio frequency test workflows. Engineers connect the sensor to the computer through USB and use supported software to configure measurements, display results, and log acquired data without adding a separate power meter to the test system. BenchVue power meter and sensor software supports instrument connection, control, visualization, and data logging, while Standard Commands for Programmable Instruments provide a programming interface for custom automated test sequences. Internal zeroing allows the measurement baseline to be established without disconnecting the radio frequency signal, helping reduce interruptions during repetitive measurements. The sensor also supports high-speed acquisition for test sequences requiring multiple readings and internal or external triggering when measurements must be coordinated with signal events or other instruments. This architecture provides a direct path from radio frequency power detection to computer-based acquisition, enabling engineers to automate measurement sequences, collect results, apply test limits, and incorporate power measurements into broader validation and production test environments.

See Block Diagram of PC-Controlled RF Power Measurement Solution

See Block Diagram of PC-Controlled RF Power Measurement Solution

Explore Products for Our PC-Controlled RF Power Measurement Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?