The Remote Keyboard utility provides an alternate method to control FieldFox remotely, and it is used along with FieldFox Remote Display.

Usage note: Remote Keyboard Utility on this page is not officially supported by Keysight and do not have extensive error checking. It is provided as a convenience. The self-extracting zipped file must be executed to extract the installation file.

Installation Requirement:

  • FieldFox Keyboard requires Keysight IO Libraries to work together. Go to www.keysight.com/find/iosuite and follow the links to install the free software.
  • Establish a LAN connection between the FieldFox and the PC. When the connection is established you will have IP addresses for the FieldFox.

 

To use this remote keyboard utility:

  1. Download FieldFox_Keyboard.zip from below.
  2. Execute FieldFox_Keyboard from the folder. The FieldFox Remote Keyboard window will appear on the PC.
  3. Click Connect button at the bottom left of the user interface.
  4. Enter FieldFox IP address and click Connect. A window dialog will pop-up upon successful connection.

 

Keysight는 가능한 최신 버전을 사용하는 것을 권장하며, 최신 버전에는 현재 사용 가능한 가장 최신 버그 수정 및 보안 패치가 포함되어 있습니다.
릴리스 날짜 버젼 버전 설명
2013-10-20 1.0 Zip file contain FieldFox Remote Keyboard setup file
릴리스 날짜 버젼
2013-10-20 1.0
Version Description
Zip file contain FieldFox Remote Keyboard setup file

다운로드 방법

  • Click the download button, select file, save and unzip.

설치 방법

  • Please read the installation instruction guide from above.

라이센스

  • Does Not Require a License

Installs on: PC

운영 체제

  • Other Windows

선결 조건

  1. FieldFox Keyboard requires Agilent IO Libraries to work together. Go to www.agilent.com/find/iosuite and follow the links to install the free software.
  2. LAN connection between FieldFox and PC.

지원되는 계측기

  • N9912A, N9923A, N9913A, N9914A, N9915A, N9916A, N9917A, N9918A, N9925A, N9926A, N9927A, N9928A, N9935A, N9936A, N9937A, N9938A
사용 가능한 소프트웨어 버전이 없습니다.
SHOW MORE