Вы искали эту информацию? Посмотреть другие результаты поиска:

 

Связаться с экспертом

Техническая поддержка

Электронные измерения

Поддержка по номеру модели:

Уточнить список

убрать все фильтры

По теме

По типу содержания

По типу оборудования

226-250 из 397

Упорядочить:
How do I connect external sensors to the U2300A Series Data Acquisition (DAQ) devices?
External sensors can be connected to the U2300A Series Data Acquisition (DAQ) devices through the U2901A or U2902A terminal block….

FAQ 2008-09-24

Why should I use the U2802A Thermocouple input device?
The U2802A Thermocouple input device offers you a complete temperature measurement solution when used with data acquisition (DAQ) devices….

FAQ 2008-09-24

When using the U2300A Series DAQ devices, how many channels can the Measurement Manager (AMM) display?
The Measurement Manager (AMM) can display all 16 or 64 channels depending on the model of the U2300A Series DAQ device selected….

FAQ 2008-09-24

Where can I get the terminal pin configuration for each model of the U2300A Series USB Data Acquisition (DAQ) devices?
The terminal pin configuration for each model of the U2300A Series USB Data Acquisition (DAQ) devices can be found in the User’s Guide….

FAQ 2008-09-24

Can the Measurement Manager (AMM) display more than 10 channels for synchronization?
No, the Measurement Manager (AMM) cannot display more than 10 channels for synchronization….

FAQ 2008-09-22

How do I connect the 33210A or 33220A to a PC via the USB port?
Install IO Libraries. Connect instrument. When prompted select “display a list of known drivers…”

FAQ 2008-09-01

Can I Perform Open/Short Test Using 34980A?
Yes. There are two ways you can setup using the 34980A to perform this test.

FAQ 2008-06-25

Can I assign names to switches when using the L4490A/L4491A?
Yes. At the web interface, right click on the switch to assign a name.

FAQ 2008-04-07

Ca Keysight build my custom L4490A/L4491A solution?
Please visit "/find/AD-systems" or see Keysight’s Channel Partners and Solution Providers at "/find/channelpartner"

FAQ 2008-04-07

Do the L449XA switch mounting kits come with screws?
Yes, they come with screws to mount bracket to switch tray, Torx T20 (M4).

FAQ 2008-04-07

Can I record the L4490A/L4491A I/O traffic?
Yes, select the "System Overview" button in the web browser to "Generate Report".

FAQ 2008-04-07

Does the L449XA have universal AC power input?
Yes, 100 Vac to 240 Vac +/- 10%, 50-60Hz.

FAQ 2008-04-07

How does the L4490A/L4491A switch verification work?
The L4490A/L4491A reads back the electronic position from the switch and issues an error if it fails to close.

FAQ 2008-04-04

Does Keysight offer L449XA mounting brackets for Keysight switches?
Yes, see data sheet.

FAQ 2008-04-04

Does the L4490A/L4491A have LED indicators?
The L4490A/L4491A provides LED drive signals on the distribution boards.

FAQ 2008-04-04

Can I mount a fan in the L449XA mainframe for cooling?
Yes, there is a fan mounting location on the rear panel for a 60mm (50mm mounting hole-to-hole spacing).

FAQ 2008-04-04

How many multiport switches fit in the L449XA?
The L4490A can support up to 8 multiport switches. The L4491A can support 16 multiport switches.

FAQ 2008-04-04

How does the L449XA switch closure counter work?
It counts each operation of the switch (open + close) and is stored in non-volatile memory of the instrument.

FAQ 2008-04-04

What options should I order with my switches when using the L4490A/L4491A?
See the data sheet for recommended switch options.

FAQ 2008-04-04

Can I add another 34945EXT to the L449XA?
The L4491A option 002 is recommended if an additional 34945EXT is required.

FAQ 2008-04-04

Does the L449XA switch tray support Keysight RF switches?
Yes, see data sheet.

FAQ 2008-04-04

Are any of the L4491A mounting rails removable?
Yes, the L4491A mounting bays can be removed or a pre-drilled bottom plate is available by ordering option 006.

FAQ 2008-04-04

Why does the L4490A/L4491A mainframe have two front panels?
The L4490A/L4491A comes with an inside panel for mounting components or connectors and an outside panel for silk screening.

FAQ 2008-04-04

Does the L449XA mainframe have an RF shielding specification?
There is no spec for RF shielding.

FAQ 2008-04-04

How do I use the L449XA web browser?
Connect the L4490A directly to your computer or the network using the LAN interface. See complete answer for details.

FAQ 2008-04-04

Назад 1 2 3 4 5 6 7 8 9 10 ... Следующие