Choose a country or area to see content specific to your location
애플리케이션 노트
High-resolution imaging has been the primary feature that attracted the researchers’ attention to scanning probe microscopy yet there are still a number of outstanding questions regarding this function of scanning tunneling microscopes and atomic force microscopes. Here I would like to address a few related issues starting with AFM imaging of alkane layers on graphite. Normal alkanes (chemical formula CnH2n+2) are linear molecules with a preferential zigzag conformation of the -CH2- groups. The terminal -CH3 groups are slightly larger than -CH2- groups but more mobile. At ambient conditions the alkanes with n=18 and higher are solid crystals (melting temperature of C18H38 – 28°C) with the chains oriented practically vertical to the larger faces of the crystals. Such surface of the C36H74 crystal, which is formed of -CH3 groups, was examined in contact mode, and the AFM images revealed the periodical arrangement of these groups 1 . It has been known for a long time that on the surface of graphite the alkane molecules are assembled in lat-laying lamellar structures, in which the fully extended molecules are oriented along three main graphite directions, Fig. 1. This molecular order is characterized by a number of periodicities: the 0.13nm spacing between the neighboring carbon atoms, the 0.25nm spacing between the -CH2- groups along the chain in the zigzag conformation, the 0.5nm interchain distance inside the lamellae and the lamellae width—the length of the extended CnH2n+2 molecule. The latter varies from 2.3nm for C18H38 to 49.5nm for C390H782 (the longest alkane synthesized).
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.