Choose a country or area to see content specific to your location
애플리케이션 노트
When Hewlett-Packard introduced the HP 8903B audio analyzer more than two decades ago, it quickly became the industry standard because of its unprecedented performance and features for its time. Its enduring popularity, even after Keysight Technologies inherited HP’s measurement business in 1999, made compatibility with the 8903B a high priority in the design of Keysight’s next generation audio analyzer. The Keysight U8903A is not only designed as a replacement for the 8903B, it also includes up-to-date features such as FFT analysis, making it ideally suited for the demands of modern audio test.
To ensure that migrating from the 8903B to the U8903A is as effortless as possible, Keysight has taken steps to ensure physical and features compatibility. For example, the U8903A not only fits into the same 3U rack space, it also has the same power-up conditions as its predecessor.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.