Choose a country or area to see content specific to your location
애플리케이션 노트
Best Solution for LF Noise Measurement
Keysight E4727B (Advanced Low-Frequency Noise Analyzer; A-LFNA) allows you to measure the LF (Low Frequency) noise of semiconductor devices very easily. The E4727B consists of hardware and software. The user can measure LF noise by just entering the expected measurement conditions and the software will then set all parameters of hardware optimally. However, there are many challenges with LF noise measurement due to environmental noise surrounding the device under test. The noise source of environmental noise is mechanical machines, instruments, mobile phone antenna, grounding issues of the system, etc. It can be very difficult to find and isolate the specific root cause of the environmental noise. This Application Note shows tips on how to improve the environment noise for LF noise measurement. In addition, the powerful environmental noise remover “Auto Denoise” is introduced.
콘텐츠 잠금 해제
무료 가입
*Indicates required field
감사합니다!
귀하의 양식이 성공적으로 제출되었습니다.
Note: Clearing your browser cache will reset your access. To regain access to the content, simply sign up again.
×
판매 문의 부탁드립니다.
*Indicates required field
감사합니다!
A sales representative will contact you soon.