E18-5jiq1
CVSS:
7.5 (AV:N/AC:L/Au:N/C:P/I:P/A:P)
False Positive:
f
Variants:
1
Year:
2018
Description
This strike exploits an Error-Based SQL injection vulnerability in Joomla! Component EkRishta 2.10. The vulnerability is caused by insufficient validation of user input on HTTP requests which are used to create SQL queries. Successful exploitation could allow an attacker to see the database information on the target server.