E20-11o31
CVSS:
9.8 CVSS:3.1/AV:N/AC:L/PR:N/UI:N/S:U/C:H/I:H/A:H
False Positive:
t
Variants:
3
Year:
2020
Description
This strike exploits a command injection vulnerability in IBM Spectrum Protect Plus. The vulnerability is due to a combination of missing authentication of the hostname uri and a lack of input sanitization for injection or invalid characters in the hostname parameter. When an attacker sends an HTTP POST request to "/emi/api/hostname", command execution can occur.