E19-0mde1
CVSS:
8.8 CVSS:3.0/AV:N/AC:L/PR:N/UI:R/S:U/C:H/I:H/A:H
False Positive:
f
Variants:
1
Year:
2018
Description
This strike exploits a vulnerability in Apple Safari Webkit. Specifically the vulnerability exists in the BytecodeGenerator::hoistSloppyModeFunctionIfNecessary method. It is possible to craft Javascript in such a way that allows for an object to be passed as the property variable directly as a string to the op_get_direct_pname handler without being properly validated. This can lead to a denial of service in the browser application or potentially allow for remote code execution to occur.
CVE
https://code.google.com/p/google-security-research/issues/detail?id=1665