Choose a country or area to see content specific to your location
Application Notes
Introduction
Urban driving situations often require a great deal of stop-and-go traffic. Meanwhile, the engine is still running using fuel and producing carbon emissions. A start-stop system’s design increases fuel efficiency; it turns off the engine when not in use. For example, if the driver has stopped at a traffic light, the start-stop system stops the engine. As soon as the light turns green and the driver releases the brake pedal, the start-stop starter motor gets the signal to restart the engine. When the driver presses the gas pedal, the car moves away quickly and reliably.
Automatic Start-Stop Testing Process
Testing the start-stop system requires test solutions of the highest caliber of speed, performance, and accuracy to recreate the power signal produced in a car during regular operation. Rigorous test requirements are required to ensure the proper functioning of the vehicle. Every single test must perform to the highest of set standards to ensure the safety of its passengers.
Unlock Content
Sign up for free
*Indicates required field
Thank you
Your form has been successfully submitted.
Your access will reset once your browser cookie expires, or browser cache is cleared. To regain access to the content, simply sign-in again.
×
Please have a salesperson contact me.
*Indicates required field
Thank you
A sales representative will contact you soon.