Wir denken, das dies die Seite ist, die Sie sehen wollten..
Stattdessen Suchergebnisse ansehen:
Können wir Ihnen behilflich sein?
Empfohlene Suchanfragen
No product matches found - System Exception
Passende Inhalte
Beam Directing And Reflecting Optics
Optics to split, bend and reflect the laser beam make layout easier and complete your system
Beam directing and reflecting optics simply reflect, bend or translate the beam, but do not typically modify the polarization, except for polarizing beam splitters. For example, mirrors, cube corners and retroreflectors are attached to objects that move in order to keep the weight down on the moving object (instead of mounting the interferometer on the moving object).
- Mirrors are usually attached to the moving object to reflect the beam back into the interferometer, but they can also be used to arbitrarily bend the beam.
- Cube corners reflect, or return, the laser beam parallel to the incoming path. They cannot be used to control the angle of reflection. The angle of reflection is fixed so that the outgoing beam is parallel to the incoming beam. Cube corners have no housing.
- Retroreflectors are the same as cube corners, but come with a housing.
- Beam benders usually deflect the beam at angles, such as 90 degrees.
- Manipulators are a special category of beam benders. They allow the beam to be easily translated or angled and give more precise control over the beam position.
- Beam splitters divide a laser beam into multiple beams. The listed percentage tells you the percentage of power of the beam that is split off of the main path. The split path is typically at 90 degrees to the main path.
- Polarizing beam splitters separate the two frequencies of the laser beam into a reference and a measurement path. Beam power is split equally between the two paths.
- Vacuum compatible means that the optic has been designed to minimize outgassing and will function in a vacuum environment. Vacuum compatible optics are primarily used in E‑beam direct write applications where the entire exposing machine and positioning stage must be placed in a vacuum.
If you do not see what you are looking for, please use the Contact Us link in the upper right hand corner of this page so that we can discuss custom optics.
Learn more about Laser Interferometer Position Measurement Systems
Find The Model That's Right For You
Sie haben bereits eines dieser Produkte?
Zum technischen Support
Vorsch.
The Keysight 10725A 50% beam splitter is designed for beam diameters of 9 mm or less. This bare optic requires a user supplied mount.
The Keysight 10713B 1-inch cube corner (retroreflector) can be used as the measurement reflector for linear measurements. This bare optic requires a user supplied mount.
The Keysight 10704A retroreflector (cube corner) reflector is a measurement reflector for single-beam measurements. It is mounted and designed for beam diameters of 6 mm or less.
The Keysight 10707A bends the incoming beam at a 90-degree angle. It is mounted and designed for beam diameters of 6 mm or less.
The Keysight 10713C 1/2 inch cube corner reflector can be used as the measurement reflector for linear measurements. This bare optic requires a user supplied mount.
Weiter
Protect Your Innovation Investment
Featured Resources
Want help or have questions?