MIPI A-PHY Automotive SerDes Receiver Test Software

Keysight empfiehlt die Verwendung der aktuellen Version, die die neuesten verfügbaren Fehlerbehebungen und Sicherheitspatches enthält.
Kostenlos Trial
Veröffentlichungsdatum Version Versionsbeschreibung
2025-06-24 1.2.0.7 - A new feature has been added that checks for available software updates. If an update is available, a notification. - Added new properties to reports and the report summary table: "Timestamp", "FW Compatibility", "Spec Deviations", "Calibrations Used", "Comments". - New user interface for the About dialog.
Veröffentlichungsdatum Version
2025-06-24 1.2.0.7
Version Description
- A new feature has been added that checks for available software updates. If an update is available, a notification. - Added new properties to reports and the report summary table: "Timestamp", "FW Compatibility", "Spec Deviations", "Calibrations Used", "Comments". - New user interface for the About dialog.

Wie geht das Herunterladen

  • Click the Download button. You are forwarded to the BitifEye download page.
  • Click on the download icon on the right and then on "Download installer file".
  • Save the file to a folder on your PC.

How to Install

  • Navigate to the folder with the downloaded  file.
  • Double-click the file to run the installer.

 

Lizenzierung

Installs on: PC

Betriebssystem

  • Windows 10 (64-bit) English, version 1809 or newer

Voraussetzungen

  • Keysight IO Libraries Suite 18.1 or newer
  • Microsoft .NET Framework 4.8 or newer

Wie geht das Herunterladen

  • Click the Download button.
  • Save the file to a folder on your PC.

How to Install

  • Navigate to the folder with the downloaded  file.
  • Double-click the file to run the installer.

 

Lizenzierung

Dokumentation

Installs on: PC

Betriebssystem

  • Windows 10 (64-bit) English, version 1809 or newer

Voraussetzungen

  • Keysight IO Libraries Suite 18.1 or newer
  • Microsoft .NET Framework 4.8 or newer
SHOW MORE