How to Shorten RF Power Measurement Test Time

Peak Power Meter
+ Peak Power Meter

Optimize RF Power Measurement Speed

Reducing radio frequency (RF) power measurement time requires selecting measurement settings that match the signal level, signal type, required resolution, and accuracy target. The measurement system consists of a power meter and compatible RF power sensor connected to the signal under test. The meter acquires the sensor output and processes it into the selected power result. Measurement speed can be affected by the number of samples or readings used for a result, the averaging applied to those readings, the selected measurement mode, and the way results are transferred or displayed. The test configuration should therefore begin with the expected signal characteristics and required measurement result, then apply only the amount of processing necessary to obtain that result.

For automated measurements, the instrument configuration also determines the time required to acquire, process, and return each result. Measurement-speed settings can be adjusted according to the required power level and the amount of averaging needed to achieve the specified reading stability. Buffer configuration can be used when multiple results need to be collected before transfer, while the selected result format and units affect how measurement data are returned to the controlling system. A production or automated test sequence can then execute repeated measurements using the optimized acquisition settings, minimizing unnecessary processing and data-transfer overhead while retaining the measurement functions required by the test.

RF Power Measurement Speed Optimization Solution

Reducing RF power measurement test time requires configuring the acquisition and result-processing settings to match the signal and required measurement accuracy. Keysight PM2-class peak power meter can be configured for different measurement-speed requirements, while the connected power sensor determines the signal response and measurement characteristics. Optimization can include selecting an appropriate measurement-speed setting, configuring the measurement buffer for repeated readings, controlling the amount of averaging used, and choosing an efficient result format and unit. These settings can reduce unnecessary acquisition and transfer time in automated sequences while preserving the power measurement functions required by the test.

Block Diagram of RF Power Measurement Speed Optimization Solution

How to Shorten RF Power Measurement Test Time

Explore Products in Our RF Power Measurement Speed Optimization Solution

Discover Resources and Insights

Additional Resources for RF Power Measurement Speed Optimization

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?