How to Program Multi-Channel RF Signal Generators

Essential Analog Signal Generator
+ Essential Analog Signal Generator

Program Independent RF Channels

Programming a multi-channel radio frequency signal generator requires commands that address each channel independently while preserving shared instrument-level settings. Engineers configure source parameters such as frequency, power, modulation, and output state for each channel, then apply common settings such as reference configuration where required. This approach allows one instrument to support multiple stimulus paths without treating every output as a separate signal source.

The test setup connects the signal generator to a controller through the supported remote interface and sends channel-specific source and output commands. Each channel can be configured with its own carrier settings and radio frequency output state, while shared nodes manage functions that apply across the instrument. This supports automated multi-channel setup for receiver test, component characterization, phase-coherent stimulus, and repeated validation where manual front-panel configuration would be slow or error-prone.

Multi-Channel Programming Solution

Program multi-channel radio frequency signal generators by addressing each source and output channel through remote commands and applying shared instrument settings where needed. The solution uses a Keysight Analog Signal Generator to support automated configuration of multiple radio frequency channels from a single instrument. Engineers can program frequency, power, modulation, and radio frequency output state per channel while managing common reference-related settings across the device. This enables repeatable setup for multi-path receiver stimulus, component testing, phase-coherent source configuration, and automated test systems that require consistent channel-by-channel control.

See Block Diagram of Multi-Channel Programming Solution

How to Automate Multi-Channel Signal Generator Setup Block Diagram

Explore Products for Our Multi-Channel Programming Solution

Discover Resources and Insights

Additional Resources for Multi-Channel Programming

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?