Layer 1-3 Network Test Products Catalog

Validate your underlying network infrastructure and devices to ensure secure, reliable performance, and connectivity while meeting industry conformance and compliance standards.

L1-3 Product Catalog

Layer 4-7 Network Test Products Catalog

Identify security gaps, performance bottlenecks, and interoperability issues with solutions that deliver insights to help you balance cybersecurity with application performance and experience.

Product Catalog

Full Network Test Across All Layers

Test functionality from the physical layer through the application layer, including software defined networking (SDN) and network function virtualization (NFV). We help you ensure data flows through your network and devices as it was designed to.

Layer 1

Validate your transceiver innovations and high-speed digital designs across all product development stages — design and simulation, analysis, debug, and compliance test.

Layers 2/3

Assess complex topologies with thousands of network devices including SDN/NFV, emulate sophisticated traffic flows, and conduct stress tests under a variety of network conditions.

Network Test Solution Icon

Layers 4–7

Create realistic customer modeling scenarios with network testing software to test and emulate network and applications at scale and to measure the quality of wired converged multi-play services.

Thoroughly Test Your Solutions

Building or deploying a new network appliance does not need to be stressful. Ensure your network and its appliances are tested at every level using the most realistic traffic scenarios.

Security

Simulate the widest variety of the latest attacks mixed with volumes of legitimate traffic to validate performance under the most realistic conditions.

Wi-Fi Networks

Completely test Wi-Fi IoT, Wi-Fi, and heterogeneous networks (HetNets) from the core to customer-facing managed services.

Cellular + 5G Networks

Create and measure the quality of 5G, LTE, and VoLTE multi-play services from the edge to the core to customer-facing managed services.

Automate Your Network Test Processes And Environments

Automation Solutions that Integrate Your Test Environment

Organizations today face a host of challenges that impact their ability to remain competitive in a world where the pace of change has accelerated exponentially. Their core goal, however, has not changed: to deliver high quality products and services with faster time to market. To achieve that, they look to automation to accelerate testing.  

The solution to increasing equipment utilization in the lab & network and accelerating functional validation & performance characterization is to automate everything. The key to a long-lasting automation solution is to select the right tools, processes, and people that will define a solution that works for today but with the future in mind.

Keysight Desktop Screen

Network Test Products

IxVerify

Validate Your Chip Design
The cost of fixing bugs after chip ‘tape-out’ can run into the millions of dollars. Reduce risk by testing during the pre-silicon stage. Push your design with high volumes of Ethernet and TCP/IP protocol traffic using hundreds of predefined packet templates. Run hundreds of virtualized test ports at once and dynamically shape traffic to ensure zero packet loss at maximum emulation speeds.

Virtual Test Solutions

Validate Virtual Networks

A top challenge for service providers is transitioning network devices to software functions. Boost the performance of virtualized functions using test tools and automated methodologies to validate and quantify the deterministic behavior of network functions virtualization (NFV) ecosystems throughout the virtual network functions (VNF) service lifecycle.

Hawkeye

Improve Your Application Performance
Get the real-time insight of your users' actual quality of experience. Create synthetic Skype, Outlook 365, and web traffic on your wired or Wi-Fi network to perform node-to-node and real-service testing to improve end-user experience.

Hawkeye is a proactive monitoring platform that ensures you are the first to know what is happening in your network.

Network Test Case Studies Image

Network Test Case Studies

Whether you are a network architect, developer, or part of an operations team, your network is always changing. Simulating realistic traffic conditions of a network or carrier to ensure efficient operations is critical to overcoming any design or operational challenge.

See how we help other innovators discover and overcome network challenges.

Want help or have questions?