How to Verify Average RF Power Across Different Signal Levels

Average Power Sensors
+ Average Power Sensors

Verify Average Power Across Signal Levels

Radio frequency (RF) devices often operate at multiple output levels as operating conditions, gain settings, or test parameters change. Engineers need to verify average power at each condition while maintaining a consistent measurement method across the test sequence. Differences in signal level can make measurement stability and sensor linearity important, particularly when comparing results across a broad range of device operating states. A sensor designed for average power measurements enables engineers to characterize these changes without requiring time-domain analysis of individual signal peaks.

The measurement setup includes an average power sensor connected to a compatible power meter and the RF source or device under test. Engineers establish the measurement frequency, perform zeroing and calibration as required, and acquire average power at each defined operating condition. Measurements can then be compared with expected output levels, design targets, or test limits to evaluate how power changes as the device moves between operating states. Using the same sensor and measurement configuration across the sequence provides a consistent basis for comparing average RF power during component characterization, functional verification, and production testing.

Average RF Power Verification Solution

Average power verification can be structured as a sequence of measurements performed while the device under test is operated at defined output conditions. Engineers configure the power meter for the measurement frequency and connect the average power sensor at the desired reference plane. The device output is then stepped through the required operating levels while the measurement system records average power at each condition. The sensor's two-path diode-pair architecture supports average-power measurements across its specified measurement range, while stored calibration, linearity, and temperature-compensation data provide correction information used by the measurement system. Engineers can compare results between operating states, identify unexpected deviations from expected power levels, and determine whether device output remains within defined limits. This workflow provides a consistent method for evaluating average RF output as operating conditions change without requiring peak-envelope or detailed time-domain analysis, supporting component development, functional verification, and repetitive production measurements.

See Block Diagram of Average RF Power Verification Solution

Block Diagram of Average RF Power Verification Solution

Explore Products in Our Average RF Power Verification Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?