How to Reduce Lead Resistance Measurement Errors

Advanced Benchtop Digital Multimeter
+ Advanced Benchtop Digital Multimeter

Separate Lead Resistance From the Measurement

Precision resistance measurements require a four-wire method when lead and contact resistance are large enough to influence the reading. One pair of leads sources test current through the device under test, while a separate sense pair measures voltage directly at the terminals so wiring resistance is excluded from the sensed voltage.

For repeatable characterization, Kelvin connections should be placed as close to the device terminals as practical, with stable contacts and an appropriate resistance range. Offset compensation can further reduce thermoelectric voltage effects in low-resistance measurements, while repeated readings help separate actual device variation from fixture or connection changes.

Precision Resistance Measurement Solution

Precision resistance characterization requires four-wire connections and stable test conditions so lead, contact, and thermal effects do not dominate the result. Keysight Advanced benchtop digital multimeters support that workflow with high-resolution resistance measurements, 2- and 4-wire measurement capability, and offset compensation that helps reduce thermoelectric effects in low-resistance work. Graphical visibility and measurement memory also help engineers compare repeated readings and identify shifts caused by the device under test versus the setup. Together, these capabilities support more repeatable resistance characterization and make it easier to evaluate small resistance changes without adding test-lead resistance directly to the measured value.

See Block Diagram of Precision Resistance Measurement Solution

Block Diagram of Precision Resistance Measurement Solution

Explore Products in Our Precision Resistance Measurement Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?