How to Recreate Complex Operating Cycles for Testing

Expert Benchtop Waveform and Function Generator
+ Expert Benchtop Waveform and Function Generator

Ensure Consistent Stimulus Across States, Transitions, and Dwell Periods

Functional testing may require a device under test (DUT) to experience an entire operating cycle rather than a single static signal condition. The stimulus can contain multiple electrical states, dwell periods, transitions, and repeated events that represent the sequence encountered during normal operation. Each portion of the cycle must occur in the intended order and for the defined duration so the complete input condition can be reproduced consistently.

The test also requires repeatable playback of the complete cycle while the DUT response is measured across each operating state and transition. Engineers may need to observe behavior during individual states, at state boundaries, or over repeated cycles while maintaining consistent stimulus timing and waveform detail. The resulting measurements can then be compared from one cycle to the next under the same functional test conditions.

Repeatable Operating Cycle Stimulus Solution

Perform the test by defining the electrical states, transitions, dwell periods, and repeated events that make up the required operating cycle and then reproducing that complete stimulus for each test run. An Expert Benchtop Waveform and Function Generator provides arbitrary waveform generation capabilities for creating and replaying complex device stimulus with controlled timing and signal detail. Individual waveform sections can represent different portions of the operating cycle and be arranged for repeatable playback without recreating the entire signal for every test condition. Waveform memory and sequence control support longer or more complex cycles, while precise waveform reproduction helps maintain the intended signal characteristics across repeated functional tests. The device response can then be captured with the appropriate measurement instrument throughout the complete cycle.

See Block Diagram of Repeatable Operating Cycle Stimulus Solution

How to Recreate Complex Operating Cycles for Testing

Explore Products for Our Repeatable Operating Cycle Stimulus Solution

Related Use Cases

contact us logo

Get in Touch with One of Our Experts

Need help finding the right solution for you?