G04-51o01
CVSS:
7.8 (AV:N/AC:L/Au:N/C:N/I:N/A:C)
False Positive:
f
Variants:
1
Year:
2004
Description
This strike exploits a vulnerability in the Snort Network Intrusion Detection System. A TCP segment with a specially crafted option fields can cause the Snort process to dereference a NULL pointer when it is running in sniffer or packet logger mode. An attacker can leverage this vulnerability to cause the Snort system on a remote target to terminate. In an attack case, the vulnerable Snort server terminates, creating a denial of service condition. Since triggering this vulnerability requires that the server to be running in sniffer or packet logger mode, the termination of Snort does not leave a target or target network unprotected because the server is already running in a non-protective mode. This vulnerability cannot be exploited for code execution.
CVE
References
http://securitytracker.com/id?1012656