Bluetooth Audio Measurement with Audio Analyzer

Applikationsberichte

Importance of Bluetooth® Audio Analysis

 The application of Bluetooth audio can be found everywhere in our normal daily lives. We use Bluetooth hands-free headsets with our cell phones to talk and to listen to music. Bluetooth audio is also available in the car infotainment system, allowing us to stream music from our cell phones to the car audio system. Hence there is need to have Bluetooth audio measurement and analysis on these devices as part of the product development, qualification and manufacturing test. Bluetooth audio is also part of the whole audio measurement and analysis ecosystem interface, which includes analog audio and digital audio.This article will focus on the Bluetooth audio measurement applications of the U8903B performance audio analyzer.